cancel
Showing results for 
Search instead for 
Did you mean: 

QUADSPI is not selectable for OCTOSPI1/2 for STM32H7A3VG in CubeMX 6.15.0

Vmanne
Associate II

Hello everybody,

Problem: I start a new project from scratch in CubeMX version 6.15.0 with STM32H7A3VG. First thing I do is to try to chose OCTOSPI1, Mode Quad-SPI. But it does not work. It's greyed out and I get the message:

"Quad SPI disabled: Quad-SPI Mode is already activated".

Same thing if I try to chose OCTOSPI2, Mode Quad-SPI.

Same thing in STMCubeIDE 1.19.

CubeMX version 6.14 allowed me to chose Quad-SPI.

Do I miss something ? Is it a bug ?

Regards

Vmanne

1 ACCEPTED SOLUTION

Accepted Solutions
KDJEM.1
ST Employee

Hello @Vmanne and @ryedwards ;

 

The issue is fixed in STM32CubeMX 6.16.0 version.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
KDJEM.1
ST Employee

Hello @Vmanne;

 

First of all thank you for posting.

Similar issue is reported here.

Internal ticket number is reported : 213708 (This is an internal tracking number and is not accessible or usable by customers).

I apologize for any inconvenience.

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Checking in on this issue.  Is there a workaround I can apply to configure QuadSPI?

 

 

KDJEM.1
ST Employee

Hello @Vmanne and @ryedwards ;

 

The issue is fixed in STM32CubeMX 6.16.0 version.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.