cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo-L4A6ZG not supported in STM32CubeMX/IDE

FVran.1
Associate

I have Nucleo-L4A6ZG board and want to use STM32CubeIDE o program it, but there is no Nucleo-L4A6ZG board in the Board Selector list. Is there a package I can install for it or I must select STM32L4A6ZG in MCU Selector and configure the rest myself?

3 REPLIES 3

Hello @FVran.1​ 

Thanks for the feedback,

You're right, It will be fixed next STM32CubeMX.

Best regards,

Nesrine

Uwe Bonnes
Principal III

It takes some time until support for new devices tickles down. If you have an FAE, perhaps ask them about pre-release. Maybe there are some.

Thank you for the quick replay!

For now I will try to use Nucleo-L496ZG profile as a reference.