cancel
Showing results for 
Search instead for 
Did you mean: 

Segger J-Link STM32H755 CM4 debugging in STM32CubeIDE

Ckerl.2
Associate II

I am trying to debug the STM32H755 within CUBEIDE but the current segger J-link drivers say that core is not supported. The segger website lists it as supported and it works without issues in their debuggers.

I am wondering if there is a workaround or way to get it working with the CM4 core?
CM7 works as expected.

Thanks.

4 REPLIES 4
Pavel A.
Super User

IIRC when you run the updater of J-Flash, it automatically finds J-Link modules (DLLs) installed in other software and updates these. Try it. Chances are it will update your CubeIDE.

 

Hi Pavel, how do I run the J-Flash updater? just running the Stm32cubeide J-Flash program doesn't seem to start any update.

Is the updater in cubeide menus? or is it a program or script in the external tools jlink folder?

Thanks!

@Ckerl.2 Download and run latest J-Link installer from Segger https://www.segger.com/downloads/jlink/

(this is a bit confusing: the J-Link installer installs a large set of various programs and utilities. Some of them are interesting and useful, others less so).

PavelA_0-1739563829806.png

 

 

Tried this, same behavior when debugging CM4 core, says device not supported and could not verify device.
Then goes to immediate hard fault.

 

Tried on windows, windows has a JLINKDLLupdater executable.
Wondering how I would get to work with linux, can I just copy over st files with latest segger.