cancel
Showing results for 
Search instead for 
Did you mean: 

The target device 'STM32N657Z0HxQ' is currently not supported by STM32CubeIDE

hamzdmr
Associate II

I selected the processor in CUBE IDE to see how much space the sd card and h264 codes will take up in ram and memory on the STM32N657Z0HxQ processor, but I got the error “The target device ‘STM32N657Z0HxQ’ is currently not supported by STM32CubeIDE”. What should I do?

hamzdmr_1-1739785518910.png

 

1 ACCEPTED SOLUTION

Accepted Solutions

@hamzdmr wrote:

I am currently using version 1.16.1,


1.16.1 does not support STM32N6 products. It was added in the V1.17.0:

From the release notes:

SofLit_0-1739796617687.png

Hope that answers your question.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

6 REPLIES 6
Andrew Neil
Super User

You didn't say what version you're using!

The STM32N series is pretty new - so you'll certainly need to be on the latest.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
ST Employee

Hello,

With STM32CubeIDE 1.17.0, I cannot see that issue. Are you sure you are using that version?

SofLit_1-1739789096520.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

You are right, I am currently using version 1.16.1, I thought the check updates I made from the Help section would work. I will update the application itself and inform you.

Have a good work

I am currently using version 1.16.1, I thought the check updates I made from the Help section would work. I will update the application itself and inform you.

Have a good work

Note that everyone can see all replies - so you don't need to repeat.

You can mention multiple people in a post using '@' ...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

@hamzdmr wrote:

I am currently using version 1.16.1,


1.16.1 does not support STM32N6 products. It was added in the V1.17.0:

From the release notes:

SofLit_0-1739796617687.png

Hope that answers your question.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.