2022-06-05 10:49 PM
Hello. I want to read multi-channel analog data (four channels) with my Nucleo-F072RB. I previously worked with Nucleo F411RE and I did not have any problems. But with F072RB, I'm so confused. When I open my board on CubeMX, I can select multi ADC1 channels (for example IN1, IN2..) but in ADC configuration I can not see "Number of Conversions" or "Rank" properties. So I can not configure the multichannel ADC. I thought maybe this board had only one configuration and so it had not allowed configuring ADCs...But when I coded two potentiometer ADC reading codes, I saw it was not working. Can you help me with this problem? Thanks in advance.
Solved! Go to Solution.
2022-06-06 9:30 AM
I just got a similar issue in my question. It may be the same issue.
It is a known issue with the MX program, they are working to fix it.
The suggestion that worked for me was to deselect all the ADC pins.
Then I generated code. And got out of the IDE.
I restarted the IDE, and and reconfigured the ADC like before. And it worked this time.
See my question "In CubeMX program for the ADC I want 4 ADC channels, but the MX program only lets me enter data for 3. How do I put in data for Rank 1?"
Hope it helps.
2022-06-05 11:52 PM
AFAIK, the F0 series Reference Manual is available. Just read it - the ADC section.
2022-06-06 7:22 AM
Thank you for your cute answer but it is not in Reference Manuel, it is about CubeMX Parameter Settings of ADC. In the picture below you can see Nucleo-F411RE ADC parameter settings when choosing multichannel ADC.
But when you use Nucleo-F072 board, you can not choose "Number of Conversion" and "Rank". Is it normal or caused by CubeMX error?
2022-06-06 9:30 AM
I just got a similar issue in my question. It may be the same issue.
It is a known issue with the MX program, they are working to fix it.
The suggestion that worked for me was to deselect all the ADC pins.
Then I generated code. And got out of the IDE.
I restarted the IDE, and and reconfigured the ADC like before. And it worked this time.
See my question "In CubeMX program for the ADC I want 4 ADC channels, but the MX program only lets me enter data for 3. How do I put in data for Rank 1?"
Hope it helps.
2022-07-22 6:51 AM
Thank you KiptonM! It worked!