2019-10-26 11:50 PM
can anyone help me with this problem cubemx is stuck at copying library file while i try to generate code for keil mdk version 5.28 cannot close the window and have to terminate the program using task manager i am using windows 10 system
2021-07-21 01:13 PM
Hello team,
I have have same problem of stuck during copy on ubuntu 21: seems like a java problem, here is my terminal log:
Exception in thread "Thread-2814" java.lang.IllegalAccessError: class parsers.FromScratchParser (in unnamed module @0x2a79781f) cannot access class com.sun.org.apache.xerces.internal.parsers.DOMParser (in module java.xml) because module java.xml does not export com.sun.org.apache.xerces.internal.parsers to unnamed module @0x2a79781f
at parsers.FromScratchParser.getDestinations(FromScratchParser.java:237)
at convertor.Convertor.generate(Convertor.java:354)
at com.st.microxplorer.plugins.projectmanager.model.ToolchainGenerator.generate(ToolchainGenerator.java:370)
at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createToolChainFolders(ProjectBuilder.java:3756)
at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createProject(ProjectBuilder.java:782)
at com.st.microxplorer.plugins.projectmanager.engine.GenerateProjectThread.run(GenerateProjectThread.java:54)
----------------------------------------------------------
/usr/local/STMicroelectronics/STM32Cube/STM32CubeMX$ java --version
openjdk 17-ea 2021-09-14
OpenJDK Runtime Environment (build 17-ea+19-Ubuntu-1ubuntu1)
OpenJDK 64-Bit Server VM (build 17-ea+19-Ubuntu-1ubuntu1, mixed mode, sharing)
Kind regards
KiranKanchi
2021-09-06 04:55 AM
Same problem here...
CubeMX version: 6.3.0
openjdk 16.0.2 2021-07-20
OpenJDK Runtime Environment (build 16.0.2+7)
OpenJDK 64-Bit Server VM (build 16.0.2+7, mixed mode)
PS. There are no 'special' characters in the filepath: '/home/schweigi/tmp/abc'
Steps to reproduce the error/failure:
o) start cubemx
o) new project with an STM32F334K8Tx
o) Project Manager -> Project Name 'x', location (I used) '/home/schweigi/tmp/abc/', Toolchain 'Makefile'
o) Generate Code
o) --> cubemx should now hang at 'Copying libraries files...'
I've also attached the corresponding log file - maybe it's helpful!?
kind regards
Bernhard
2021-09-06 08:08 AM
🙂 Found a solution in the meantime - the culprit seems to be an incompatibility with the used java version.
When I use an older java version (I tested openjdk version "11.0.12" 2021-07-20, since this version was still installed on my machine) everything works fine again...
kind regards
Bernhard
2022-01-07 03:13 AM
Ча�?то решить такую проблему помогает С�?ЯТИЕ галочки "Project manager -> Generate under root" и ввод пути к папке дл�? компил�?ции вручную.
Веро�?тно, проблема в том, что по-умолчанию дл�? компил�?ции проектов и�?пользует�?�? пака пользовател�?, им�? которого может быть напи�?ано, например, на кириллице, которую, почему-то, до �?их пор не переваривают продукты STM 🙂 Так что проблема не только �? �?имволами "&%$" и так далее, но и про�?то �? кодировкой...