Found a solution in the meantime - the culprit seems to be an incompatibility with the used java version.When I use an older java version (I tested openjdk version "11.0.12" 2021-07-20, since this version was still installed on my machine) everythi...
Same problem here...CubeMX version: 6.3.0openjdk 16.0.2 2021-07-20OpenJDK Runtime Environment (build 16.0.2+7)OpenJDK 64-Bit Server VM (build 16.0.2+7, mixed mode)PS. There are no 'special' characters in the filepath: '/home/schweigi/tmp/abc'Steps to...
As written in the initial posting from Michal: Now i am using procedure: - Reset SPI in RCC - complete init SPI but it doesnt looks like a legal procedure...Regarding the question, if this procedure is 'allowed', I found the following in ...