can anyone help me with this problem cubemx is stuck at copying library file while i try to generate code for keil mdk version 5.28 cannot close the window and have to terminate the program using task manager i am using windows 10 system
Yes i tried that also previously i was using 5.3 version(the same error persisted there, hence i updated mx to 5.4) deleted that installed 5.4 mx and since it was not working i reinstalled 5.4 but still no luck