cancel
Showing results for 
Search instead for 
Did you mean: 

MBEDTLS gray when azureRTOS is enable

aabba.1
Associate III

Hi,

why MBEDTLS cann't work with azureRTOS (Iam using stm32h7) ?

 

Thank you

4 REPLIES 4
STTwo-32
ST Employee

Hello @aabba.1 

I've not been able to reproduce this. Can you add more details about your configurations.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

  1. Select MUC STM32H7B3LIHXQ via STM32CubeMx (version 6.9.2) 
  2. MBEDTLS can be enable
  3. Enable RTOS ThreadX
  4. MBEDTLS cann't be enable

 

aabba1_1-1703708111042.png

 

Semer CHERNI
ST Employee

Hello @aabba.1 

As shown in the pop up message the MBDEDTLS is not available when AZURERTOS is activated.

SemerCHERNI_0-1704189631323.png

KR,
Semer.

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

aabba.1
Associate III

yes I understand, but why?