Is it possible to change peripheral instance name?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-03-30 4:10 AM - last edited on 2025-03-10 2:24 AM by Andrew Neil
Hi,
I'm developing some firmware having in mind a possible future need for portability. Being so, I thought about labeling pinouts on the Device Configuration Tool (DCT) and generate code (in the future, giving the same pin names to different pin groups should work).
However, I can't see a way to do the same with peripheral instances. For example, if I choose TIM6 on some uC and would like to choose (for whatever reason) TIM2 on another uC and with the same configuration, I would like to label them the same (MY_TIMER, or so) so I could adapt the firmware more easily.
In short, I wanted to generate from DCT or Cube MX the same peripheral configurations, with the ability to change the peripherals without changing the label.
Is this possible?
Thanks in advance
- Labels:
-
STM32CubeMX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-03-30 4:36 AM
Don't think that this is possible for generated code. Some board support package (BSP) drivers demonstrate how it could be done with hand-written code: https://github.com/STMicroelectronics/STM32CubeF4/blob/master/Drivers/BSP/STM32F4-Discovery/stm32f4_discovery.h
hth
KnarfB