I cannot use SW pins as GPIO for some reason
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-11-24 4:04 AM
I swear i was able to do this in the past but then ...... then i updated from 6.3.0 to cubeMX 6.6.1.
Maybe thats the reason, maybe not .
Im using a stm32f105RBT6
When i flash the chip and remove the stlink both PA13 and PA14 are stuck into some idle 1,3V floating state instead of toggle each second like PA10
I am not sure where should i look to be sure pin SW functions are not on.
Setting up pins as GPIOs in cubeMX
Code inside main, simple GPIO toggle
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_ADC1_Init();
MX_CAN1_Init();
MX_TIM1_Init();
MX_TIM2_Init();
MX_TIM3_Init();
MX_TIM4_Init();
MX_TIM7_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
HAL_Delay(1000);
HAL_GPIO_TogglePin(uC_OUT_01_GPIO_Port, uC_OUT_01_Pin);
HAL_GPIO_TogglePin(uC_OUT_02_GPIO_Port, uC_OUT_02_Pin);
HAL_GPIO_TogglePin(uC_OUT_03_GPIO_Port, uC_OUT_03_Pin);//Only thisone works
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
I am flashing the release version wchih is not supposed to be using SW debugging pins at all..... i ran out of ideas
Solved! Go to Solution.
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-11-24 5:20 AM
Hello @Javier Muñoz ,
Maybe this could give you some hints if you are in this case :
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-11-24 4:09 AM
CUBEMX generated GPIO init looks okay to me
/** Configure pins as
* Analog
* Input
* Output
* EVENT_OUT
* EXTI
*/
void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOC, uC_OUT_19_Pin|uC_AUX_19_Pin|uC_OUT_18_Pin|uC_AUX_18_Pin
|uC_OUT_17_Pin|uC_AUX_17_Pin|uC_OUT_16_Pin|uC_AUX_12_Pin
|uC_OUT_11_Pin|uC_OUT_06_Pin|uC_AUX_06_Pin|uC_OUT_05_Pin
|uC_AUX_05_Pin, GPIO_PIN_RESET);
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOA, uC_AUX_16_Pin|uC_OUT_15_Pin|uC_AUX_15_Pin|uC_OUT_14_Pin
|uC_AUX_14_Pin|uC_OUT_13_Pin|uC_AUX_13_Pin|uC_OUT_12_Pin
|uC_OUT_04_Pin|uC_AUX_04_Pin|uC_OUT_03_Pin|uC_AUX_03_Pin
|uC_LED_POWER_Pin|uC_OUT_02_Pin|uC_OUT_01_Pin, GPIO_PIN_RESET);
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOB, uC_AUX_11_Pin|uC_OUT_10_Pin|uC_AUX_10_Pin|uC_OUT_09_Pin
|uC_OUT_08_Pin|uC_AUX_08_Pin|uC_OUT_07_Pin|uC_AUX_07_Pin
|uC_OUT_20_Pin|uC_AUX_20_Pin, GPIO_PIN_RESET);
/*Configure GPIO pins : PCPin PCPin PCPin PCPin
PCPin PCPin PCPin PCPin
PCPin PCPin PCPin PCPin
PCPin */
GPIO_InitStruct.Pin = uC_OUT_19_Pin|uC_AUX_19_Pin|uC_OUT_18_Pin|uC_AUX_18_Pin
|uC_OUT_17_Pin|uC_AUX_17_Pin|uC_OUT_16_Pin|uC_AUX_12_Pin
|uC_OUT_11_Pin|uC_OUT_06_Pin|uC_AUX_06_Pin|uC_OUT_05_Pin
|uC_AUX_05_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
/*Configure GPIO pins : PAPin PAPin PAPin PAPin
PAPin PAPin PAPin PAPin
PAPin PAPin PAPin PAPin
PAPin PAPin */
GPIO_InitStruct.Pin = uC_AUX_16_Pin|uC_OUT_15_Pin|uC_AUX_15_Pin|uC_OUT_14_Pin
|uC_AUX_14_Pin|uC_OUT_13_Pin|uC_AUX_13_Pin|uC_OUT_12_Pin
|uC_OUT_04_Pin|uC_AUX_04_Pin|uC_OUT_03_Pin|uC_AUX_03_Pin
|uC_OUT_02_Pin|uC_OUT_01_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*Configure GPIO pins : PBPin PBPin PBPin PBPin
PBPin PBPin PBPin PBPin
PBPin PBPin */
GPIO_InitStruct.Pin = uC_AUX_11_Pin|uC_OUT_10_Pin|uC_AUX_10_Pin|uC_OUT_09_Pin
|uC_OUT_08_Pin|uC_AUX_08_Pin|uC_OUT_07_Pin|uC_AUX_07_Pin
|uC_OUT_20_Pin|uC_AUX_20_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/*Configure GPIO pin : PtPin */
GPIO_InitStruct.Pin = uC_LED_POWER_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(uC_LED_POWER_GPIO_Port, &GPIO_InitStruct);
/*Configure GPIO pin : PtPin */
GPIO_InitStruct.Pin = uC_IN04_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
HAL_GPIO_Init(uC_IN04_GPIO_Port, &GPIO_InitStruct);
/*Configure GPIO pins : PCPin PCPin PCPin */
GPIO_InitStruct.Pin = uC_IN08_Pin|uC_IN03_Pin|uC_IN07_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
/*Configure GPIO pin : PtPin */
GPIO_InitStruct.Pin = uC_IN02_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
HAL_GPIO_Init(uC_IN02_GPIO_Port, &GPIO_InitStruct);
/*Configure GPIO pins : PBPin PBPin PBPin */
GPIO_InitStruct.Pin = uC_IN06_Pin|uC_IN01_Pin|uC_IN05_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-11-24 5:20 AM
Hello @Javier Muñoz ,
Maybe this could give you some hints if you are in this case :
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-11-24 5:35 AM
Thanks @Herve PIERROT , ill give it a look to AN4989 and get back to you with my findings.
What troubles me is... i never had this problem before untill now, and im using both SW pins as alternative functions in the same hardware with other projects.
Ill downgrade to cubeMX 6.3.0 also
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-11-24 6:33 AM
@Herve PIERROT , i already fixed it , there is nothing wrong with cubeMX nor the firmware package.
I just deleted the project, generated everything again with cubeMX 6.6.1, copied my libraries and now its fine.
Something went wrong when i updated CUBEMX and regenerated the progect, i believe the issue was in the files autogenerated by cubeMX at that point.... but i dont have the time to figure out what, anyway everything is working now.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-11-24 6:36 AM
perfect, thanks for the feedback, most important is that it works now :thumbs_up: