‎2021-08-20 3:26 AM
‎2021-08-20 4:35 AM
To me looks reasonable. Your input signal clips at negative, and the "wobble" you see is the effect of limited number of samples per source period.
JW
‎2021-08-20 5:12 AM
If the source signal frequency(100kHz) is low , the ADC sample then look fine.
‎2021-08-20 5:22 AM
Try to sample it at the same sampling frequency ratio, i.e. 100kHz / 2MHz * 5.1Msps = 255ksps.
JW
‎2021-08-20 7:44 AM
There is no change, it is till distorted
‎2021-08-20 8:00 AM
What is still distorted? 100kHz signal sampled with 255ksps?
That's my point, you can't see a "nice" sine if you interpolate only a few points (in your case 2.55 in average) per period.
JW
‎2021-08-23 5:28 AM
@Community member​
Thank you, I understand , I have interpolated it and got the proper sine wave. I would rather want to implement dual interleaved mode ADC. Please do you have a sample code for stm32F303RE
‎2021-08-23 6:10 AM
No, sorry.
JW