2020-12-16 8:24 AM
Please see the images attached:
Project Manager.
Error Message after project generation.
STM32 Cube MX logfile with Error Message.
CUBE MX Version: STM32Cube MCU Package for STM32F4 Series 1.25.2
Keil version: 5.27
Thanks for your time.
Best Regards,
Luke
Solved! Go to Solution.
2020-12-16 8:52 AM
Hi LMyle.1,
Thanks for quick reply, as I can from the .log file you have attached, you're using an unsupported Java version (Detected Java Version = 15.0.1) which is the reason behind this issue.
Actually JAVA Versions 7, 9, 10, 12 and upper are not supported. For more details about the CubeMX software requirements, please refer to the STM32CubeMX User Manual.
To solve the issue, you have to uninstall the current Java in your machine and install a supported version:
Hope this will solve your problem.
Khouloud.
2020-12-16 8:32 AM
Hello LMyle.1,
Could you please share your .ioc file and the .log file, it will be helpful to check the issue.
Thanks in advance,
Khouloud.
2020-12-16 8:40 AM
2020-12-16 8:42 AM
2020-12-16 8:52 AM
Hi LMyle.1,
Thanks for quick reply, as I can from the .log file you have attached, you're using an unsupported Java version (Detected Java Version = 15.0.1) which is the reason behind this issue.
Actually JAVA Versions 7, 9, 10, 12 and upper are not supported. For more details about the CubeMX software requirements, please refer to the STM32CubeMX User Manual.
To solve the issue, you have to uninstall the current Java in your machine and install a supported version:
Hope this will solve your problem.
Khouloud.
2020-12-16 8:58 AM
Great I will try this thank you
2020-12-16 9:03 AM
Please click on the Select as Best button on my reply if it solved your issue. This will help other members of the community find this solution more quickly