2024-09-06 2:32 AM
Hi guys
I want to generate a time base by a general purpose timer interrupt (TIM6) on a F334 with low level library. I do not know why, I get init functions fine but no interrupt request handler is generated, nowhere.
It should be very simple, I thought, but I did nothing with STM32 for a longer time. I remember to did this (and more...) with old HAL library years ago, but even though if I select HAL in advanced settigs, I get nothing better.
I use the last firmware package version (CubeMX says its version 1.11.5) and tried many things before, including that here:
https://community.st.com/t5/stm32cubemx-mcus/how-to-generate-callback-functions-in-stm32cubemx/td-p/130320
So I come up here, maybe someone else know what is going wrong here? I attach the cubemx file, maybe somebody can ivestigate what I've forgotten?
Solved! Go to Solution.
2024-09-06 3:01 AM - last edited on 2024-09-06 3:03 AM by mƎALLEm
After posting this, I found the irq handler in the stm32f3xx.it file. Ok, problem is solved (I hope).
2024-09-06 3:01 AM - last edited on 2024-09-06 3:03 AM by mƎALLEm
After posting this, I found the irq handler in the stm32f3xx.it file. Ok, problem is solved (I hope).
2024-09-06 5:20 AM
If you know the name of a function, you can use Search -> File... to find out where it is.
2024-09-06 12:21 PM
Yes, this is in fact my biggest problem during using the ll library.
I had started with assembler an avrs many years ago, no problem with understanding the programming manual, even though it is a huge bunch.
But knowing the right function names is a challenge, even though you have the low layer description read and do not exactly know what you are looking for. But I think I will get it...even I will maybe have to come back multiple times here. A lot of experienced people seems to be here.