cancel
Showing results for 
Search instead for 
Did you mean: 

How to change the Pull-up/Pull-down behavior in the stm32CubeMx Software.

FSchm.7
Associate

 I am using Linux Linux kubuntu 22.10 5.19.0-26-generic and when I click on the GPIO Pull-up/Pull-down column elements nothing happens except the color of the row changes.

1 ACCEPTED SOLUTION

Accepted Solutions
Karl Yamashita
Principal

You have to scroll down or drag the configuration window up a little bit to see the parameters

0693W00000WLM4KQAX.png

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

View solution in original post

3 REPLIES 3
MM..1
Chief III

Click on System Core and GPIO.

Karl Yamashita
Principal

You have to scroll down or drag the configuration window up a little bit to see the parameters

0693W00000WLM4KQAX.png

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.
FSchm.7
Associate

@Community member​  thanks a lot I just didn't see the scroll bar