2023-04-12 6:49 AM
I am relatively new to using the STM32 family and I am trying to use the USART on a STM32C011J4M6 device without success.
Initially I am just trying to send out a single character using the lines
uint8_t TxData[] = {'@'};
HAL_UART_Transmit(&huart1, TxData, 1, 10);
after USART1 has been set up by CubeMX.
When it runs however, as soon as it tries to write to the Transmit Data Register, the processor resets. I have verified where it is going wrong by stepping through the disassembly - all the registers seem to be set up correctly but immediately on executing the STR instruction to write the character to 0x40013828 (USART1 TDR) it jumps to the reset handler.
I have been using STM32F042K6 and other devices up until now and the same code behaves correctly in those, exactly as expected.
I'm not sure what I am doing wrong so can anyone point to what it might be? If I remove the HAL_UART_Transmit() then the rest of the code runs (although it is just toggling a GPIO pin at the moment).
Thanks for any advice.
2023-04-12 6:56 AM
Hello @Neiliow ,
uint8_t TxData[] = "@";
HAL_UART_Transmit(&huart1, TxData, 1, 10);
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-04-12 7:27 AM
Thanks Foued but that's not where the problem is. The '@' character is getting to the correct place and it fails when it is trying to write that into the Transmit Register. I can trace the disassembled program right up to that point so it is getting the character to send out. The problem happens when I write to TDR, it doesn't matter what data I try to write to it - '@' or anything else.
Neil
2023-04-12 7:43 AM
The processor shouldn't reset.
Double check board, make sure the UART TX pin isn't connected to anything that would reset the system, or cause a short or brown-out type event.
Code lacks any broader context.
Is this a chip with low pin count or pins bonded to multiple IO outputs or function?
2023-04-12 8:12 AM - edited 2023-11-20 8:24 AM
The Tx pin is just connected to an oscilloscope and the chip is in a breadboard with the only connections being its power rails, an LED on a GPIO pin and the ST-Link on the SWD pins.
There isn't much code at the moment other than what was generated by Cube MX. The chip is an 8-pin device so the pins have multiple functions but only USART1 and SWD are enabled.
However you have got me wondering now - the TxD pin is also shared with nRST so maybe that is what's happening. When TxD goes low it is seeing that as a reset. I'll have a look into it. Thanks for the hint.
2023-04-12 8:20 AM
Yes, super low pin count device. Watch what else is bonded to pin.
Attach minimal / buildable project demonstrating issue as a ZIP file.
2023-04-12 8:39 AM
2023-04-12 9:12 AM - edited 2023-11-20 8:25 AM
Update - I found in the Cube Programmer a setting to disable the reset input on that pin and setting it to 2 as above stops the processor from resetting on a Tx.
I still can't see any data coming out of the pin yet but that is probably a different problem. I think it's closer to working than it was before.
Thanks for your inspiration!