2019-12-23 2:28 PM
C:\Users\marti\AppData\Local\Arm\Packs\Keil\STM32G4xx_DFP\1.1.0\Drivers\STM32G4xx_HAL_Driver\Src\stm32g4xx_ll_fmc.c(176): error: #20: identifier "FMC_NORSRAM_TypeDef" is undefined
HAL_StatusTypeDef FMC_NORSRAM_Init(FMC_NORSRAM_TypeDef *Device, FMC_NORSRAM_InitTypeDef *Init)
C:\Users\marti\AppData\Local\Arm\Packs\Keil\STM32G4xx_DFP\1.1.0\Drivers\STM32G4xx_HAL_Driver\Src\stm32g4xx_ll_fmc.c(176): error: #20: identifier "FMC_NORSRAM_InitTypeDef" is undefined
HAL_StatusTypeDef FMC_NORSRAM_Init(FMC_NORSRAM_TypeDef *Device, FMC_NORSRAM_InitTypeDef *Init)
C:\Users\marti\AppData\Local\Arm\Packs\Keil\STM32G4xx_DFP\1.1.0\Drivers\STM32G4xx_HAL_Driver\Src\stm32g4xx_ll_fmc.c(201): warning: #223-D: function "__FMC_NORSRAM_DISABLE" declared implicitly
__FMC_NORSRAM_DISABLE(Device, Init->NSBank);
C:\Users\marti\AppData\Local\Arm\Packs\Keil\STM32G4xx_DFP\1.1.0\Drivers\STM32G4xx_HAL_Driver\Src\stm32g4xx_ll_fmc.c(204): error: #20: identifier "FMC_MEMORY_TYPE_NOR" is undefined
if (Init->MemoryType == FMC_MEMORY_TYPE_NOR)
2019-12-23 2:40 PM
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* <h2><center>© Copyright (c) 2019 STMicroelectronics.
* All rights reserved.</center></h2>
*
* This software component is licensed by ST under BSD 3-Clause license,
* the "License"; You may not use this file except in compliance with the
* License. You may obtain a copy of the License at:
* opensource.org/licenses/BSD-3-Clause
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1);
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
Error_Handler();
}
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
2019-12-23 2:45 PM
2019-12-23 2:55 PM
Need to make sure the FMC modules is enabled in stm32g4xx_hal_conf.h
Check also command line defines.
2019-12-24 3:43 AM
Hi, thanks to the Input of clive1 i found out that you have to enable the SRAM Module in stm32g4xx_hal_conf.h
/*#define HAL_SRAM_MODULE_ENABLED */
--->
#define HAL_SRAM_MODULE_ENABLED
Seems to be an CUBEMX BUG
Thanks a lot
Thomas
2020-01-03 1:37 AM
Hello @Thomas1s , Please share your ioc file.
Issue not reproduced on my side.
Best Regards,
Khouloud.
2020-01-16 2:26 AM
Hello, did you receive the ioc file? I have the same issue in G473 in Keil, where the Cube generated code won't compile in stm32g4xx_ll_fmc.c until I uncomment the line with #define HAL_SRAM_MODULE_ENABLED in the stm32g4xx_hal_conf.h header.
2020-01-16 8:22 AM
Hello @Andreja Kostic , no ! could you please share yours ?
Did you create a project from CubemX then generated code on Keil , when building did you find errors ? please give me more details .
Thanks,
Khouloud
2020-01-22 1:46 AM
Hello @Khouloud ZEMMELI, sorry for the delay. I sent a description of the issue and few problematic files to you via private message.
Unfortunately, I forgot to mention tool versions.
I used STM32CubeMX version 5.5.0.
The Keil versions are:
µVision V5.29.0.0
C Compiler: Armcc.exe V5.06 update 6 (build 750)
Assembler: Armasm.exe V5.06 update 6 (build 750)
Linker/Locator: ArmLink.exe V5.06 update 6 (build 750)
Library Manager: ArmAr.exe V5.06 update 6 (build 750)
Hex Converter: FromElf.exe V5.06 update 6 (build 750)
CPU DLL: SARMCM3.DLL V5.29.0.0
Dialog DLL: TCM.DLL V1.36.5.0
Target DLL: UL2CM3.DLL V1.163.0.0
Dialog DLL: TCM.DLL V1.36.5.0
and the STM32G4XX_DFP is version 1.1.0.
2020-10-28 11:18 AM
Hello everyone, I return to the topic. Has anyone found the source of this issue?
I am creating the project from scratch in Keil, then I add the STMCubeMx from the RTE administrator, without initializing any peripherals or modules, I just click on "Generate code". And I have the same issue with HAL_SRAM_MODULE_ENABLED.
Thanks!