cancel
Showing results for 
Search instead for 
Did you mean: 

Where in CubeMX can I check the Wait States?

Ricko
Senior III

Hi,

I am using the STM32U5G9VJT6Q and in CubeMX I configured the clock to the full 160MHz for all busses including the core (first screenshot). According to the documentation for 160MHz I need to set 4 Wait States for those speeds and VCORE voltage needs to be in Range 1 (second screenshot).

Two questions if someone could please help:

1. after setting the clock in MX, where can I check that the wait states have been set correctly (in MX - not programmatically, debug or other ways) ?

2. in MX, where do I set the VCORE? If it is set automatically, where can I check that it is set correctly (in MX - not programmatically, debug or other ways)?

Thank you :)

Ricko

Ricko_0-1741045992307.png

 

Ricko_1-1741046086361.png

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

Both of those are in the RCC tab.

TDK_0-1741052735664.png

 

VCORE is "Power Regulator Voltage Scale"

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
TDK
Super User

Both of those are in the RCC tab.

TDK_0-1741052735664.png

 

VCORE is "Power Regulator Voltage Scale"

If you feel a post has answered your question, please click "Accept as Solution".

Thank you @TDK