cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, i'm a beginner and need some help. I bought a nucleo g474 Board and followed 2 startup how tos. Keil + Cubemx. When i produce the initialisation code i always get the error in the stm32g4xx_ll_fmc.c file Does anybody know what im doing wrong?

Thomas1s
Associate II

C:\Users\marti\AppData\Local\Arm\Packs\Keil\STM32G4xx_DFP\1.1.0\Drivers\STM32G4xx_HAL_Driver\Src\stm32g4xx_ll_fmc.c(176): error: #20: identifier "FMC_NORSRAM_TypeDef" is undefined

 HAL_StatusTypeDef FMC_NORSRAM_Init(FMC_NORSRAM_TypeDef *Device, FMC_NORSRAM_InitTypeDef *Init)

C:\Users\marti\AppData\Local\Arm\Packs\Keil\STM32G4xx_DFP\1.1.0\Drivers\STM32G4xx_HAL_Driver\Src\stm32g4xx_ll_fmc.c(176): error: #20: identifier "FMC_NORSRAM_InitTypeDef" is undefined

 HAL_StatusTypeDef FMC_NORSRAM_Init(FMC_NORSRAM_TypeDef *Device, FMC_NORSRAM_InitTypeDef *Init)

C:\Users\marti\AppData\Local\Arm\Packs\Keil\STM32G4xx_DFP\1.1.0\Drivers\STM32G4xx_HAL_Driver\Src\stm32g4xx_ll_fmc.c(201): warning: #223-D: function "__FMC_NORSRAM_DISABLE" declared implicitly

  __FMC_NORSRAM_DISABLE(Device, Init->NSBank);

C:\Users\marti\AppData\Local\Arm\Packs\Keil\STM32G4xx_DFP\1.1.0\Drivers\STM32G4xx_HAL_Driver\Src\stm32g4xx_ll_fmc.c(204): error: #20: identifier "FMC_MEMORY_TYPE_NOR" is undefined

  if (Init->MemoryType == FMC_MEMORY_TYPE_NOR)

9 REPLIES 9
Thomas1s
Associate II
/* USER CODE BEGIN Header */
/**
  ******************************************************************************
  * @file           : main.c
  * @brief          : Main program body
  ******************************************************************************
  * @attention
  *
  * <h2><center>&copy; Copyright (c) 2019 STMicroelectronics.
  * All rights reserved.</center></h2>
  *
  * This software component is licensed by ST under BSD 3-Clause license,
  * the "License"; You may not use this file except in compliance with the
  * License. You may obtain a copy of the License at:
  *                        opensource.org/licenses/BSD-3-Clause
  *
  ******************************************************************************
  */
/* USER CODE END Header */
 
/* Includes ------------------------------------------------------------------*/
#include "main.h"
 
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
 
/* USER CODE END Includes */
 
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
 
/* USER CODE END PTD */
 
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
 
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
 
/* USER CODE END PM */
 
/* Private variables ---------------------------------------------------------*/
 
/* USER CODE BEGIN PV */
 
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
/* USER CODE BEGIN PFP */
 
/* USER CODE END PFP */
 
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
 
/* USER CODE END 0 */
 
/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{
  /* USER CODE BEGIN 1 */
 
  /* USER CODE END 1 */
  
 
  /* MCU Configuration--------------------------------------------------------*/
 
  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();
 
  /* USER CODE BEGIN Init */
 
  /* USER CODE END Init */
 
  /* Configure the system clock */
  SystemClock_Config();
 
  /* USER CODE BEGIN SysInit */
 
  /* USER CODE END SysInit */
 
  /* Initialize all configured peripherals */
  /* USER CODE BEGIN 2 */
 
  /* USER CODE END 2 */
 
  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
    /* USER CODE END WHILE */
 
    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */
}
 
/**
  * @brief System Clock Configuration
  * @retval None
  */
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
  /** Configure the main internal regulator output voltage 
  */
  HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1);
  /** Initializes the CPU, AHB and APB busses clocks 
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
  RCC_OscInitStruct.HSIState = RCC_HSI_ON;
  RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }
  /** Initializes the CPU, AHB and APB busses clocks 
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 
  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
  {
    Error_Handler();
  }
}
 
/* USER CODE BEGIN 4 */
 
/* USER CODE END 4 */
 
/**
  * @brief  This function is executed in case of error occurrence.
  * @retval None
  */
void Error_Handler(void)
{
  /* USER CODE BEGIN Error_Handler_Debug */
  /* User can add his own implementation to report the HAL error return state */
 
  /* USER CODE END Error_Handler_Debug */
}
 
#ifdef  USE_FULL_ASSERT
/**
  * @brief  Reports the name of the source file and the source line number
  *         where the assert_param error has occurred.
  * @param  file: pointer to the source file name
  * @param  line: assert_param error line source number
  * @retval None
  */
void assert_failed(uint8_t *file, uint32_t line)
{ 
  /* USER CODE BEGIN 6 */
  /* User can add his own implementation to report the file name and line number,
     tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
  /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
 
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

Thomas1s
Associate II

0690X00000BuvwrQAB.png0690X00000BuvwmQAB.png0690X00000BuvwhQAB.png

Need to make sure the FMC modules is enabled in stm32g4xx_hal_conf.h

Check also command line defines.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Thomas1s
Associate II

Hi, thanks to the Input of clive1 i found out that you have to enable the SRAM Module in stm32g4xx_hal_conf.h

/*#define HAL_SRAM_MODULE_ENABLED  */

--->

#define HAL_SRAM_MODULE_ENABLED 

Seems to be an CUBEMX BUG

Thanks a lot

Thomas

​Hello @Thomas1s​ , Please share your ioc file.

Issue not reproduced on my side.

Best Regards,

Khouloud.

Hello, did you receive the ioc file? I have the same issue in G473 in Keil, where the Cube generated code won't compile in stm32g4xx_ll_fmc.c until I uncomment the line with #define HAL_SRAM_MODULE_ENABLED in the stm32g4xx_hal_conf.h header.

​Hello @Andreja Kostic​ , no ! could you please share yours ?

Did you create a project from CubemX then generated code on Keil , when building did you find errors ? please give me more details .

Thanks,

Khouloud

Hello @Khouloud ZEMMELI​, sorry for the delay. I sent a description of the issue and few problematic files to you via private message.

Unfortunately, I forgot to mention tool versions.

I used STM32CubeMX version 5.5.0.

The Keil versions are:

µVision V5.29.0.0

C Compiler:        Armcc.exe       V5.06 update 6 (build 750)

Assembler:         Armasm.exe       V5.06 update 6 (build 750)

Linker/Locator:    ArmLink.exe       V5.06 update 6 (build 750)

Library Manager:   ArmAr.exe       V5.06 update 6 (build 750)

Hex Converter:     FromElf.exe       V5.06 update 6 (build 750)

CPU DLL:              SARMCM3.DLL         V5.29.0.0

Dialog DLL:        TCM.DLL             V1.36.5.0

Target DLL:            UL2CM3.DLL          V1.163.0.0

Dialog DLL:        TCM.DLL             V1.36.5.0

and the STM32G4XX_DFP is version 1.1.0.

JTánt.1
Associate II

Hello everyone, I return to the topic. Has anyone found the source of this issue?

I am creating the project from scratch in Keil, then I add the STMCubeMx from the RTE administrator, without initializing any peripherals or modules, I just click on "Generate code". And I have the same issue with HAL_SRAM_MODULE_ENABLED.

Thanks!