2021-05-27 2:55 PM
Hi, I've generated a project using STM32CubeMX for the STM32G030C8Tx and I've included FREERTOS. The heap_x file is not listed in the GPDSC file. I think this is a bug, note someone else appears to have had the same issue here: Topic: Error undefined reference to `pvPortMalloc and `vPortFree' | Sysprogs
Attached is my .ioc file and GPDSC file (I had to change it to a txt file to upload).
2021-06-01 6:21 AM
Hi @Martin Franke
Let me be sure that I understand the issue, is that Heap_x.c files are not generated in project folder?
In my case ,when I load your ioc and generate using STM32CubeMX , Heap_1.c to Heap_5.c are generated under :
Middlewares\Third_Party\FreeRTOS\Source\portable\MemMang\
Please tell me if I miss something?
Houda
2021-06-01 9:10 AM
Hello @Houda GHABRI,
Thanks for looking into this. The files are generated correctly, but there is no reference to them in the gpdsc file. I'm using VisualGDB with CubeMX and when I generate a new project it doesn't automatically reference them since it pulls all its references from the gpdsc file. It's not a major bug since I can manually add them but might be really frustrating for someone. It wasn't immediately obvious to me where the problem was when I began the project.
Thanks,
Martin
2021-06-02 5:51 AM
Hi @Martin Franke ,
Thanks I catch the point.
The issue is reproduced and internal ticket is submitted to STM32CubeMX development team to be fixed as soon as possible.
Houda
2021-06-02 11:58 AM
Hello @Houda GHABRI ,
Thank you very much for taking time to submit this to the development team.
Martin
2021-06-03 1:04 AM
Hi @Martin Franke ,
Thanks to you for bringing this error to our attention.
Houda