HAL Peripheral MSP Init. Why does STM32CubeIDE generated code not include a call to this function?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-12-11 5:52 AM
I made a UART project in STM32CubeIDE. Cube generated the necessary UART initialisation code and created UART_INIT() function (or something like that) in main(). The project worked.
Then I decided to add DMA. I regenerated the code and couldn't find DMA initialisation in UART_INIT(). I found out that this code was generated in another file in UART_MSP_INIT() function (or something like that). My questions are:
- Why does Cube generate this code in another file? Why not in UART_INIT() or DMA_INIT() in main()?
- Do I have to explicitly call UART_MSP_INIT() in main() by myself? And why doesn't Cube do it automatically?
- I found out that GPIO alternate function configuration (for UART) was also made in UART_MSP_INIT(). But I did't explicitly call UART_MSP_INIT() before using DMA. So why did UART work if the pins were not configurated?
Solved! Go to Solution.
- Labels:
-
STM32CubeIDE
-
STM32CubeMX
-
UART-USART
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-12-11 6:15 AM
The HAL files under Drivers are used for several chips. That code doesn't change. The chip/project configuration maps to files in Core/Src. Thats main() calling MX_USART2_UART_Init(); for example. That function fills a setup struct and calls a somehow generic HAL function HAL_UART_Init() which in turn calls HAL_UART_MspInit() in Core/Src stm32f0xx_hal_msp.c which inits the underlying components like the GPIOs.
Try debug-stepping through the init code to get the idea.
MSP = MCU Support Package
hth
KnarfB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-12-11 6:09 AM
> Why does Cube generate this code in another file? Why not in UART_INIT() or DMA_INIT() in main()?
Who knows, it is what it is. But they should NOT be called from within UART_Init, so it doesn't make perfect sense to locate them there.
> Do I have to explicitly call UART_MSP_INIT() in main() by myself? And why doesn't Cube do it automatically?
It's called within HAL_UART_Init and should not be called by yourself. Cube does call it automatically.
> I found out that GPIO alternate function configuration (for UART) was also made in UART_MSP_INIT(). But I did't explicitly call UART_MSP_INIT() before using DMA. So why did UART work if the pins were not configurated?
Because it was called and they were configured.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-12-11 6:15 AM
The HAL files under Drivers are used for several chips. That code doesn't change. The chip/project configuration maps to files in Core/Src. Thats main() calling MX_USART2_UART_Init(); for example. That function fills a setup struct and calls a somehow generic HAL function HAL_UART_Init() which in turn calls HAL_UART_MspInit() in Core/Src stm32f0xx_hal_msp.c which inits the underlying components like the GPIOs.
Try debug-stepping through the init code to get the idea.
MSP = MCU Support Package
hth
KnarfB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-12-11 6:36 AM
Before explicitly calling HAL_UART_MspInit() in main() I actually made a breakpoint in it to find out if the function is called or not. And the program didn't stop there. That's why I assumed that this function is not called automatically. Maybe I just made a mistake.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-12-11 7:22 AM
You're not supposed to call the *_MspInit functions. HAL has a default "do nothing" implementation defined "weak" for the linker. For the peripherals in use, those are "overloaded" by the implementation in stm32f0xx_hal_msp.c. Some call it software design, others bloatware.