Flash size setting for QSPI and OCTOSPI convention in STM32CubeMX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-05-21 2:32 AM
I have a question about the convention in STM32CubeMX to specify Flash size for QSPI and OCTOSPI.
The two application notes do not state the same thing.
Application note for QUADSPI says: "Flash size is 16 Mbytes => number of bytes in Flash memory = 2[FSIZE+1] = 2[23+1] => FSIZE = 23"
Application note for OCTOSPI says:Which would mean that 24 stands for 16bytes.
So which one is true and which one should I use for the OCTOSPI
- Labels:
-
Documentation
-
OctoSPI
-
QSPI
-
STM32CubeMX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-08-25 10:49 AM
I have basically the same question.
I am using the OCTOSPI1 controller on an ST32H723 with an MX25L3233 part (4megaBYTE).
If I configure DEVSIZE to "21" which docs say should allow access to 2^22 addresses, I cannot access beyond 2megabyte.
If i configure DEVSIZE to "22", I can access the entire 4 megabytes.
So how should DEVSIZE be configured?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-08-25 12:30 PM
QUADSPI and OCTOSPI are different controllers.
You're reporting behaviour as described in the OCTOSPI App Note
21 = 2 MB
22 = 4 MB
23 = 8 MB
24 = 16 MB
DEVSIZE is a 5-bit field in OCTOSPI_DCR1, where 2^(DEVSIZE+1) is the size.
The initialization code takes the DeviceSize field and does the subtraction
So Init.DeviceSize = 24 defines a 16MB device
STM32Cube_FW_H7_V1.8.0\Drivers\STM32H7xx_HAL_Driver\Src\stm32h7xx_hal_ospi.c
HAL_OSPI_Init
/* Configure memory type, device size, chip select high time, clocked chip select high time, delay block bypass, free running clock, clock mode */
MODIFY_REG(hospi->Instance->DCR1,
(OCTOSPI_DCR1_MTYP | OCTOSPI_DCR1_DEVSIZE | OCTOSPI_DCR1_CSHT | OCTOSPI_DCR1_CKCSHT |
OCTOSPI_DCR1_DLYBYP | OCTOSPI_DCR1_FRCK | OCTOSPI_DCR1_CKMODE),
(hospi->Init.MemoryType | ((hospi->Init.DeviceSize - 1U) << OCTOSPI_DCR1_DEVSIZE_Pos) |
((hospi->Init.ChipSelectHighTime - 1U) << OCTOSPI_DCR1_CSHT_Pos) |
(hospi->Init.ClkChipSelectHighTime << OCTOSPI_DCR1_CKCSHT_Pos) |
hospi->Init.DelayBlockBypass | hospi->Init.ClockMode));
The memory devices themselves just tend to mask to the address bit counts they support, and the image you can read simply wraps within the address space.
In the STM32H74x/75x parts the last 32-bytes of the part have issues, I think there's an errata on that.
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
‎2021-08-25 3:26 PM
Wow, an QSPI device in SOP16(W) that Arrow has in-stock!!
MX25L3233FMI
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
‎2021-08-26 5:10 AM
Thank you for the explanation. i apprear to have been over thinking it a bit.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-09-07 2:42 PM
Have these working on the bench. Might make an external loader for Keil / ST tools
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
‎2023-11-16 1:26 AM
Again, thank you Tesla DeLorean.