2024-09-19 1:46 PM - last edited on 2024-10-01 7:39 AM by Andrew Neil
Hello,
Since the latest release of CubeMX (6.12.1), I have been encountering syntax errors related to the "FLASH.ld" file. This issue only arises when I generate code while setting the Toolchain/IDE to CMake. I am using STM32H753IIKx. It seems that CubeMX does not specify which RAM to use when setting the Toolchain/IDE to CMake.
I have also included the FLASH.ld file that was generated for your reference.
Thanks for your help.
Solved! Go to Solution.
2024-10-19 3:19 AM
2024-10-24 6:45 AM
Thanks a lot Grzegorz,
Your answer helped me on two separate project ! Hope the next version of cubeMX come soon
2024-11-01 12:31 AM
How long it will take to fix?
Now is 2024-11-1
2024-11-04 6:02 AM
Agreed. This is not great and surely can't be hard to fix. 4/11/24
2024-11-08 11:06 PM
9/11/24, problem still not fixed!
2024-11-17 5:45 AM
17/11/24, not fixed yet
2024-11-17 10:39 AM
You are very naive. Some bugs are not fixed in years (like 10 byte USB descriptor). Looks like very Indian software house product.
2024-11-22 3:38 AM
Thanks a lot!
at least I am able to compile.
But actually I am wondering myself how the CubeMX will be tested before a release or will it be tested at all...
I am trying to create a simple Blinky example to work since 2 days and actually I am running from one bug to another.
2024-11-25 1:00 PM
Certified ST software quality moment.
Imagine how trivial it is to test this thing before pushing it to thousands of users.
Please, increase you QA budget at least.
This is a nightmare...
2024-11-25 1:35 PM
It's been at least TWO MONTHS since this major, show-stopping bug was reported. WTF ST? Get your act together. This is appalling.