cancel
Showing results for 
Search instead for 
Did you mean: 

FLASH.ld syntax error when upgrading to CubeMX v6.12.1

OmidES
Associate II

Hello,

Since the latest release of CubeMX (6.12.1), I have been encountering syntax errors related to the "FLASH.ld" file. This issue only arises when I generate code while setting the Toolchain/IDE to CMake. I am using STM32H753IIKx. It seems that CubeMX does not specify which RAM to use when setting the Toolchain/IDE to CMake.

I have also included the FLASH.ld file that was generated for your reference.

 

Thanks for your help.

27 REPLIES 27
Andrew Neil
Evangelist III

Thanks a lot Grzegorz,

 

Your answer helped me on two separate project ! Hope the next version of cubeMX come soon

How long it will take to fix?

Now is 2024-11-1

Agreed. This is not great and surely can't be hard to fix. 4/11/24

9/11/24, problem still not fixed!

17/11/24, not fixed yet

You are very naive. Some bugs are not fixed in years (like 10 byte USB descriptor). Looks like very Indian software house product.

Thanks a lot!

at least I am able to compile.

But actually I am wondering myself how the CubeMX will be tested before a release or will it be tested at all...

I am trying to create a simple Blinky example to work since 2 days and actually I am running from one bug to another.