cancel
Showing results for 
Search instead for 
Did you mean: 

FLASH.ld syntax error when upgrading to CubeMX v6.12.1

OmidES
Associate II

Hello,

Since the latest release of CubeMX (6.12.1), I have been encountering syntax errors related to the "FLASH.ld" file. This issue only arises when I generate code while setting the Toolchain/IDE to CMake. I am using STM32H753IIKx. It seems that CubeMX does not specify which RAM to use when setting the Toolchain/IDE to CMake.

I have also included the FLASH.ld file that was generated for your reference.

 

Thanks for your help.

45 REPLIES 45
Andrew Neil
Super User

Now a recognised problem:

https://community.st.com/t5/stm32cubemx-mcus/issue-with-linker-script-in-stm32cubemx-6-12-1/td-p/733007

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Thanks a lot Grzegorz,

 

Your answer helped me on two separate project ! Hope the next version of cubeMX come soon

How long it will take to fix?

Now is 2024-11-1

Agreed. This is not great and surely can't be hard to fix. 4/11/24

9/11/24, problem still not fixed!

17/11/24, not fixed yet

You are very naive. Some bugs are not fixed in years (like 10 byte USB descriptor). Looks like very Indian software house product.

Thanks a lot!

at least I am able to compile.

But actually I am wondering myself how the CubeMX will be tested before a release or will it be tested at all...

I am trying to create a simple Blinky example to work since 2 days and actually I am running from one bug to another.

RichardS1
Associate II

Certified ST software quality moment.

Imagine how trivial it is to test this thing before pushing it to thousands of users.

Please, increase you QA budget at least.

This is a nightmare...

cyclebot
Associate II

It's been at least TWO MONTHS since this major, show-stopping bug was reported. WTF ST? Get your act together. This is appalling.