cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX - V6.12.0 CAN-FD Transciever Delay Compensation & Auto Retransmission

CZuercher_Ilm
Associate II

Hi,

I'm currently using STM32CubeMX V6.12.0 to initialise the peripherals on an STM32H753 processor, and I had a couple of questions:

1. How do I enable & then configure the CAN Transciever Delay Compensation within CubeMX?

2. Is there a mechanism for limiting the number of auto-retransmissions in the event of a CAN Error? I currently have that option unchecked but when doing bench-top testing it's clogging up the processor and causing it to run slowly.

 

Many Thanks,

 

Crispin

0 REPLIES 0