cancel
Showing results for 
Search instead for 
Did you mean: 

Error in generated cyabs_freertos_helpers.c file

nobody
Associate II

Hi,

When I generate code with the STN32CubeIDE 1.14.0 and CubeMX 6.10.0 RC9 then it does now the __WEAK in the cyabs_freertos_helpers.c file. My workaround is at the moment to include directly in that file the "stm32u5xx_hal.h" then it works till the next time i generate code.

How can I fix that properly or is that only fixable inside the cubeMX code generator?
Why is the /* USER CODE BEGIN Includes */ not working? Is that only working for some special files?

Thanks in advance
nobody

0 REPLIES 0