2024-09-23 5:24 AM
As long as my .ioc file has the lines
VP_EXTMEM_MANAGER_SIG_Activate_EXTMEM.Mode=Activate_EXTMEM
VP_EXTMEM_MANAGER_SIG_Activate_EXTMEM.Signal=EXTMEM_MANAGER_SIG_Activate_EXTMEM
in it, CubeIDE and CubeMX will be unable to open it with the error:
Cannot invoke "java.util.List.iterator()" because "destList" is null.
Deleting these two lines make it work. I am using 6.12.1 with an STM32H7R3I8Tx.
2024-09-23 8:33 AM
I figured out the real issue:
I wanted to use NOR flash on the listed MCU. The way I set it up was that the first 2 MB of the chip was used for the boot sector, and the remaining 62 MB of the chip was used for the application sector. This causes the issue, as the first 2 MB are empty when they should be reserved from the boot sector. I just added that to the application section too and made it "All access not permitted" which should work. This still gives an error but allows the program to run.