2018-09-11 9:58 PM
Hi All,
I am trying to set up an ADC channel on a specific pin on the STM32F207ZETx; PA0 (pin 34) and I have come across a pretty "big" problem.
When I set the pin and go to configure the pin, the "ADC1" button does not respond to a click and doesn't "look" like it usually does. I have attempted this on different STM32F2 MCUs with the same result. Everything seems fine with the F1 and F3 chips when I set them up.
There is no icon, so to speak, on the button and nothing happens when I click it. To make things worse, once a project is saved like this it cannot be re-opened - it becomes corrupt.
I am using version 4.26.1
For reference this is what it is supposed to look like when there are no issues:
I wasn't sure where to post this, so if it is in the wrong thread I apologise in advance, any solutions would be greatly appreciated!
2018-09-12 10:44 AM
Dear @alex_embedded ,
Many thanks for your feedback! This is the convenient place to report any potential bug you encounter.
I have reproduced the issue you're seeing and I will highlight it internally for further investigation.
We will answer you ASAP.
Thanks!
Khouloud.
2018-09-12 10:48 AM
Hi @alex_embedded ,
Just note that the new release of the STM32CubeMX tool (V4.27.0) is now available under ST website.
Link:
Khouloud.
2018-09-12 10:53 AM
FYI CubeMX 4.26.1 is NOT recognizing that an update is available, server side database might need updating.
2018-09-12 10:56 AM
Thanks @Community member for bringing this to our attention.
I will report this to our teams immediately.
Khouloud.
2018-09-12 7:38 PM
Hi All,
Just a quick update,
CubeMX did not find the new version but I did download it and install it manually. My project has been migrated to the new version and I can confirm that the ADC setup appears to be working!
I have no tried to save yet, but I assume it'll save without any troubles. If not I'll let you all know!
Thanks for the help!
2018-09-13 1:04 AM
Thanks for the update. If you have any feedback, do not hesitate to share it here ;)
Khouloud.
2018-09-17 9:08 AM
@Khouloud GARSI database looks to have been updated over weekend, 4.26.1 has recognized availability of update. Thanks
2018-09-17 9:12 AM
You're always welcome Clive!