cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX FMC Import Errors

MRobe.1
Associate III

Hi

See attached IOC.  When I import this to a clean (just created in CubeMX, version shown in attached) project the FMC is, incorrectly, flagged as having errors.  I do not know if other aspects are imported correctly or not.

Method:

  • start CubeMX
  • File > New Project
  • Select STM32F429NIH6
  • Import Project (select attached project)
  • Complains that the FMC settings (Mode) is all wrong (which I don't believe it to be and which works when I change these manually).
  • sometimes FMC pins show in yellow, sometimes, green after the import
  • Clock Configuration has not been imported correctly
  • incorrectly says the "only" imported aspect is RCC when, clearly, other aspects have been imported
  • Correcting the FMC and Clock import errors seems to be correct and flags no warnings (ie it seems the original settings were fine which I have proved by generating and running code on target)

Regards

 

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0