cancel
Showing results for 
Search instead for 
Did you mean: 

STM32N6570-DK Image classification Flashing error

Jayasree1414
Associate

Iam getting this error continuously while flashing. I have taken custom dataset and trained. Training is done. Deployment is done but stm32cubeide is not generating bin. I have set the board to dev mode and connected the CN6.

 

"make -j6 all" terminated with exit code 2. Build might be incomplete.

14:02:56 Build Failed. 3 errors, 5 warnings. (took 29s.939ms)

Stm32cubeide:
Java was started but returned exit code=1
-Dosgi.requiredJavaVersion=1.8
-Dosgi.instance.area.default=@user.home/STM32CubeIDE/workspace_1.19.0
-Declipse.buildId=Version 1.19.0
-DproductMaturityGrade=mm
-Djdk.http.auth.tunneling.disabledSchemes=
-XX:+UseG1GC
-XX:+UseStringDeduplication
-Xms256m
-Xmx1024m
-Djavax.net.ssl.trustStoreType=WINDOWS-ROOT
-Djava.class.path=C:\ST\STM32CubeIDE_1.19.0\STM32CubeIDE\\plugins/org.eclipse.equinox.launcher_1.6.900.v20240613-2009.jar
-os win32
-ws win32
-arch x86_64
-launcher C:\ST\STM32CubeIDE_1.19.0\STM32CubeIDE\stm32cubeide.exe
-name Stm32cubeide
--launcher.library C:\ST\STM32CubeIDE_1.19.0\STM32CubeIDE\\plugins/org.eclipse.equinox.launcher.win32.win32.x86_64_1.2.1100.v20240722-2106\eclipse_11904.dll
-startup C:\ST\STM32CubeIDE_1.19.0\STM32CubeIDE\\plugins/org.eclipse.equinox.launcher_1.6.900.v20240613-2009.jar
--launcher.overrideVmargs
-application org.eclipse.cdt.managedbuilder.core.headlessbuild
-import D:\EMBEDDED\BOARDS\STM32\STM32_PROJECT\stm32ai-modelzoo-services\application_code\image_classification\STM32N6\Application\STM32N6570-DK\STM32CubeIDE
-data C:\Users\Admin\AppData\Local\Temp\tmpcrzy99ji
-cleanBuild STM32N6570-DK_GettingStarted_ImageClassification/Debug
-vm C:\ST\STM32CubeIDE_1.19.0\STM32CubeIDE\\plugins/com.st.stm32cube.ide.jre.win64_3.4.0.202409160955/jre/bin\server\jvm.dll
-vmargs
-Dosgi.requiredJavaVersion=1.8
-Dosgi.instance.area.default=@user.home/STM32CubeIDE/workspace_1.19.0
-Declipse.buildId=Version 1.19.0
-DproductMaturityGrade=mm
-Djdk.http.auth.tunneling.disabledSchemes=
-XX:+UseG1GC
-XX:+UseStringDeduplication
-Xms256m
-Xmx1024m
-Djavax.net.ssl.trustStoreType=WINDOWS-ROOT
-Djava.class.path=C:\ST\STM32CubeIDE_1.19.0\STM32CubeIDE\\plugins/org.eclipse.equinox.launcher_1.6.900.v20240613-2009.jar
flashing.. Debug STM32N6570-DK
[returned code = 1 - FAILED]
$ cwd: ../application_code/image_classification/STM32N6/Application/STM32N6570-DK/STM32CubeIDE
$ args: STM32_SigningTool_CLI -s -bin Debug/STM32N6570-DK_GettingStarted_ImageClassification.bin -nk -t ssbl -hv 2.3 -o Debug/STM32N6570-DK_GettingStarted_ImageClassification_signed.bin
QIODevice::read (QFile, "Debug\STM32N6570-DK_GettingStarted_ImageClassification.bin"): device not open
-------------------------------------------------------------------
STM32 Signing Tool v2.20.0
-------------------------------------------------------------------

Error: binary file does not exist: Debug/STM32N6570-DK_GettingStarted_ImageClassification.bin
Available commands:

--help -h -? : Show help
--version -v : Display this program version

--binary-image -bin : Input binary image file path
--input -in Syntax 1: -bin <File_Path>
Syntax 2: -in <File_Path>

--public-key -pubk : Public keys file paths
Syntax: -pubk <File_Path{1..8}>
Note for header v1: use just one key path
Note for header v2: use 8 keys paths
--private-key -prvk : Private key file path
Syntax: -prvk <File_Path>
--password -pwd : Password of the private key
Syntax: -pwd <Password>

--image-version -iv : Image version
Syntax: -iv <Version>
Note : 1 is the default version value
--load-address -la : Load address of image
Syntax: -la <Load_Address>
--entry-point -ep : Image entry point
Syntax: -ep <Entry_Point>
--option-flags -of : Option flags of image
Syntax: -of <Option_Flags>
--algorithm -a : 1. (P-256 NIST) 2. (Brainpool 256) 3. (P-384 NIST) 4. (Brainpool 384)
Syntax: -a <2>
Note : 1- P256NIST is the default algo
--type -t : Binary Type
Syntax: -t <type>
Possible values : ssbl fsbl teeh teed teex copro

--enc-dc -encdc : Encryption derivation constant for FSBL encryption [header v2]
Syntax: -encdc <Deriv_Val>
--enc-key -enck : OEM secret file for FSBL encryption [header v2]
Syntax: -enck <Key_Path>
--output -o : Output file path
Syntax: -o <Output_File_Path>
--silent -s : Silent mode, no prompt messages

--dump-header -dump : Parse and dump image header
Syntax: -dump <File_Path>
--na-payload -nap : Non authenticated input payload path [only for header v2.1]
Syntax: -nao <Payload_Path>
--header-version -hv : Signing header version, Possible values : 1 2 2.1 2.2 2.3
Syntax: -hv <header_value>
Default value: 1 for header v1 using 1 public key
Default value: 2 for header v2 using 8 public keys
--no-keys -nk : Adding empty header without key options.
Syntax: -nk
Additional PKCS#11 commands:

--module -m : Specify a PKCS#11 module/Library path to load (dll, so, dylib)
Syntax: -m <File_Path>
--key-index -ki : List of used keys indexes in hex format.
Use 1 index for Header v1 and 8 indexes for header v2
Syntax: -ki <value>
--slot-index -si : Specify the index of the slot to use (default 0)
Syntax: -si <value>
--slot-identifier -sid : Specify the identifier of the slot to use (Optional, in decimal or hex format)
Syntax: -sid <value>
--active-keyIndex -aki : Specify th actual active key index (default 0)
Syntax: -aki <value>
Board programming failed: "Error: binary file does not exist: Debug/STM32N6570-DK_GettingStarted_ImageClassification.bin"
[returned code = 1 - FAILED]
$ cwd: ../application_code/image_classification/STM32N6/Application/STM32N6570-DK/STM32CubeIDE
$ args: STM32_Programmer_CLI -c port=swd mode=HOTPLUG sn=004200193234511233353533 --extload C:\ST\STM32CubeIDE_1.19.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.2.200.202503041107\tools\bin\ExternalLoader/MX66UW1G45G_STM32N6570-DK.stldr -w Debug/STM32N6570-DK_GettingStarted_ImageClassification_signed.bin 0x70100000
-------------------------------------------------------------------
STM32CubeProgrammer v2.20.0
-------------------------------------------------------------------

ST-LINK SN : 004200193234511233353533
ST-LINK FW : V3J16M9
Board : STM32N6570-DK
Voltage : 3.27V
SWD freq : 8000 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x486
Revision ID : Rev B
Device name : ST32N657
Device type : MCU
Device CPU : Cortex-M55
BL Version : --

Error: File does not exist: STM32N6570-DK_GettingStarted_ImageClassification_signed.bin
Board programming failed: "Error: File does not exist: STM32N6570-DK_GettingStarted_ImageClassification_signed.bin"
Board programming failed: "Error: File does not exist: STM32N6570-DK_GettingStarted_ImageClassification_signed.bin"
Board programming failed: "Error: File does not exist: STM32N6570-DK_GettingStarted_ImageClassification_signed.bin"
[INFO] : Deployment complete.
[INFO] : Please on STM32N6570-DK toggle the boot switches to the left and power cycle the board.

0 REPLIES 0