2025-07-14 8:50 AM - last edited on 2025-07-14 9:00 AM by Andrew Neil
Hi,
Thanks,
Peter
2025-07-14 9:30 AM
Hello @RongShengWang
Ensure that the project is not generated inside another project and try to change the path of your project to another directory.
BR,
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-07-16 9:02 AM
I had to check "Generate under root" checkbox in Project Manager". I did not, which wasted me 3 days to deal with many troubles caused by the simply clicking the checkbox. It should be defaulted to "Generate under root"