cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMx Export info

drake
Associate II
Posted on March 04, 2015 at 11:41

Hi

With

CubeMx

,

I can

associate

the

Label

for each

pin

of the MCU

or

only some of them

.

Exporting the

project to

TrueSTUDIO

,

I have noticed

that these

customizations

remain only

in the

.ioc

file

and are not

included in the

source code

,

even after

the import

of the project

( in TrueStudio) .

Is this correct

?

Best Regard

D.

#st32cubemx
4 REPLIES 4
stm32cube-t
Senior III
Posted on March 10, 2015 at 15:23

Yes this is correct.

This option is not yet supported.

hbarta2
Associate III
Posted on March 10, 2015 at 16:24

Please add my vote to include this feature.

An alternative and perhaps more useful feature would be to create set_XXX()/reset_XXX() functions or macros for all user named GPIO pins (where XXX is the user assigned name.)

Along with STemWin support. (But I think that propagating user names will likely be easier. ;) )

Thanks!

drake
Associate II
Posted on March 16, 2015 at 15:47

If

have to

vote

to add

this feature

I want to

give my vote

.

I believe it is

a useful

and

convenient

.

Regard

Drake

stm32cube-t
Senior III
Posted on October 11, 2015 at 23:31

Dear users,

This feature will be delivered in STM32CubeMX 4.11 coming out this month.

Best regards