2015-03-04 02:41 AM
Hi
With
CubeMx
,I can
associate
the
Label
for each
pin
of the MCU
or
only some of them
.Exporting the
project to
TrueSTUDIO
,I have noticed
that these
customizations
remain only
in the
.ioc
fileand are not
included in the
source code
,even after
the import
of the project
( in TrueStudio) .Is this correct
?
Best Regard D. #st32cubemx2015-03-10 07:23 AM
Yes this is correct.
This option is not yet supported.2015-03-10 08:24 AM
Please add my vote to include this feature.
An alternative and perhaps more useful feature would be to create set_XXX()/reset_XXX() functions or macros for all user named GPIO pins (where XXX is the user assigned name.)Along with STemWin support. (But I think that propagating user names will likely be easier. ;) )Thanks!2015-03-16 07:47 AM
If
have to
vote
to add
this feature
I want to
give my vote
.
I believe it is
a useful
and
convenient
.
Regard Drake2015-10-11 02:31 PM