cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX Issues

nadiradn
Associate
Posted on October 07, 2015 at 08:19

have you ever noticed, that pinout and clock config tabs aren't matching each other?

especially if you select Nucleo or Discovery Boards, on pinout Tab you can see pin's selected and marked properly, but Clock configuration tab doesn't reflect proper crystals ...

for STM32F4 Discovery there is an issue with clocking ratios so when you move to clock config tab mostly it is red overclocked... 

for STM32F466RET Nucleo board, it doesn't reflect 32 kHz crystal connected to the MCU PC14,PC15...

 

#stm32 #cubemx
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on October 07, 2015 at 17:02

Hi nadiradze.nikoloz,

Which version of CubeMx are you using?

-Shahrzad-

Posted on October 10, 2015 at 01:50

Yes, I did notice that in an old version of the tool.  Download the current versions of CubeMX and the F4 modules and the clock tree is correct.