cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX CANBUS LL Library Support

embeddedguy1
Associate

I have an STM32F407G discovery development kit. I activate CANBUS while doing pin configuration via CubeMX. Then in project manager > advanced settings > driver selector tab, I can select both LL library and HAL library in all options such as GPIO, DMA, USART, ADC. But when I want to select LL library for CANBUS, I see that only HAL library is available. Why is there no LL support for CANBUS in CubeMX? Is there any way to add it? I would appreciate if you can help me.

1 ACCEPTED SOLUTION

Accepted Solutions

@embeddedguy1 wrote:

Why is there no LL support for CANBUS in CubeMX? .


Because there is no support for CAN in LL at all - CubeMX cannot add support that does not exist!

The available HAL & LL support is documented in UM1725Description of STM32F4 HAL and low-layer drivers:

https://www.st.com/resource/en/user_manual/um1725-description-of-stm32f4-hal-and-lowlayer-drivers-stmicroelectronics.pdf

via: https://www.st.com/en/embedded-software/stm32cubef4.html#documentation 

You can see that there is no LL CAN support

 


@embeddedguy1 wrote:

 Is there any way to add it?


No - because it does not exist.

 

See also:

https://community.st.com/t5/stm32-mcus-products/simulink-code-generation-support-for-stm32f407g-disc1-can-bus/m-p/728438/highlight/true#M262690 

View solution in original post

4 REPLIES 4
SofLit
ST Employee

Hello,

Not all peripherals have LL driver including CAN.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
embeddedguy1
Associate

That's what I'm talking about, why do you answer just to answer?


@embeddedguy1 wrote:

Why is there no LL support for CANBUS in CubeMX? .


Because there is no support for CAN in LL at all - CubeMX cannot add support that does not exist!

The available HAL & LL support is documented in UM1725Description of STM32F4 HAL and low-layer drivers:

https://www.st.com/resource/en/user_manual/um1725-description-of-stm32f4-hal-and-lowlayer-drivers-stmicroelectronics.pdf

via: https://www.st.com/en/embedded-software/stm32cubef4.html#documentation 

You can see that there is no LL CAN support

 


@embeddedguy1 wrote:

 Is there any way to add it?


No - because it does not exist.

 

See also:

https://community.st.com/t5/stm32-mcus-products/simulink-code-generation-support-for-stm32f407g-disc1-can-bus/m-p/728438/highlight/true#M262690 

Because there is no LL driver for CAN. See this thread: https://community.st.com/t5/stm32-mcus-products/simulink-code-generation-support-for-stm32f407g-disc1-can-bus/m-p/728438/highlight/true#M262690

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.