cancel
Showing results for 
Search instead for 
Did you mean: 

[Cube OTG USB] [Minor issue]incorrectly @param description on HAL_StatusTypeDef USB_FlushTxFifo(USB_OTG_GlobalTypeDef *USBx, uint32_t num)

oneshot.triplekill
Associate II

The original param description:

 * @param num FIFO number

 *    This parameter can be a value from 1 to 15

      15 means Flush all Tx FIFOs

According to stm32h7 reference manual, it should be:

 * @param num FIFO number

 *    This parameter can be a value from 1 to 15

      16 means Flush all Tx FIFOs

:beaming_face_with_smiling_eyes:

2 REPLIES 2
Sara BEN HADJ YAHYA
ST Employee

Hello @oneshot.triplekill@qq.com​ ,

Thanks for your feedback,

This is not a CubeMX issue, the stm32h7xx_ll_usb.c file is copied and not generated by MX. I see your point, there is indeed a mismatch between the Reference manual and the usb driver file.

I am adding @Amel NASRI​  to the loop to further check this issue.

Sara.

ahaha, thanks .:beaming_face_with_smiling_eyes: