cancel
Showing results for 
Search instead for 
Did you mean: 

Can't find DAC configuration for STM32F411E-Disco in CubeIDE/CubeMX

YLiu.10
Associate

Hi,

I'm new to STM32 board and following a tutorial which uses DAC. The board I'm using is STM32F411E-Disco, and I select the board in CubeIDE to create a project.

The board 32F411EDISCOVERY - Discovery kit with STM32F411VE MCU - STMicroelectronics has a DAC but I can't find it when I try to configure the pins in CubeIDE/CubeMX.0693W00000FCmXgQAL.pngDo I miss something?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

The chip doesn't have an onboard DAC. However, the board has an audio DAC chip which is connected to the MCU and is controlled via I2S (and I2C?).

0693W00000FCme8QAD.png

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

1 REPLY 1
TDK
Super User

The chip doesn't have an onboard DAC. However, the board has an audio DAC chip which is connected to the MCU and is controlled via I2S (and I2C?).

0693W00000FCme8QAD.png

If you feel a post has answered your question, please click "Accept as Solution".