2026-01-30 3:10 AM
With CubeIDE 1.x iterative development is simple
1 Start CubeIDE and create new project. It is possible to select C++ project option at project start (without any effect)
2 With Device Configuration Tool create initial perifery config. It is possible to open second windows for it and have two separate windows side by side. Generate code.
3 Switch to first window and work with generated code
4 If need new device, switcn to second window, add new device, config it and generate code.
5 In first window regenerated code is created in sync with Configuration Tool. Convenient and logical steps. Great work!
How iterative development can be done with CubeIDE 2.0?
Solved! Go to Solution.
2026-01-30 5:14 AM - edited 2026-01-30 5:19 AM
Hello @vybor
Thank you for posting!
This article will help you to understand the new iterative development with the new CubeIDE 2.0.0
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-01-30 5:14 AM - edited 2026-01-30 5:19 AM
Hello @vybor
Thank you for posting!
This article will help you to understand the new iterative development with the new CubeIDE 2.0.0
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.