2018-08-20 1:56 PM
I am using a STM32H7 ADC in multimode. When I generate the source code with STM32CUBEMX 4.26.1 and STM32CubeH7 Firmware Package V1.3.0 / 04-July-2018, i noticed that inside MX_ADC1_Init() in main.c, the following line of code is written:
multimode.DualModeData = ADC_DMAACCESSMODE_DISABLED;
which is throwing compile time exception.
As I understand it should be
multimode.DualModeData = ADC_DUALMODEDATAFORMAT_DISABLED;
Also I noticed that STM32CubeMX IDE is showing "DMA Access Mode" on the second line in ADCs_Common_Settings which is probably is root cause of this issue
Solved! Go to Solution.
2018-09-27 7:05 AM
Hi @MaxR ,
Thanks for your feedback,
I confirm its a bug and it will be fixed in next CubeMX release,
Please feel free to contact me for further details,
Best regards,
Mohamed
2018-09-27 3:15 AM
Hi @MaxR ,
I have highlighted your request internally for further check.
One of our experts will answer you ASAP.
Khouloud.
2018-09-27 7:05 AM
Hi @MaxR ,
Thanks for your feedback,
I confirm its a bug and it will be fixed in next CubeMX release,
Please feel free to contact me for further details,
Best regards,
Mohamed