2017-04-13 7:19 AM
hi to all, i use a cubemx 4.20.1 for configure STM32L152RE; when i configure the RTC pin with alarm A i see a error handler.
indeed when the system arrived to LSE configuration i have a HAL_TIMEOUT,
can you help me?
best regards
A.
#bug #rtc #cubemx #lse-osc32-not-starting-oscillation2017-04-17 7:18 AM
Hi,
Could you please share your .ioc file to ckeck your issue?
Imen
2017-04-18 12:33 AM
Hi Imen,
in this folder you can download my ioc file
https://www.dropbox.com/sh/if8hee3py9v2u83/AAC7ZWj79C3fTbdpaBut6V5ya?dl=0
thx
Antonio
2017-04-18 3:36 AM
Hi
Buonanno.Antonio
,You have this configuration code from CubeMx:
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE
|RCC_OSCILLATORTYPE_LSE;
You should removethe
RCC_OSCILLATORTYPE_HSI o
scillator
that you don't need.This issue is fixed in the CubeMx version 4.1 and you should first EDIT the .ioc file and REMOVEtheRCC.OscillatorType that you don't need
E.g: remove this line
RCC.OscillatorTypeHSI=RCC_OSCILLATORTYPE_HSI
Then re-generate the project, this will resolve your problem.
Imen
2017-04-18 6:49 AM
Hi Imen thanks for your answer,
i create a new file ioc, i see that the system crashes when i active LSE in RTC/LCD source MUX, if i use LSI i don't have problem.
Antonio
2017-08-18 11:47 AM
Hello,
I have same problem with ver. 4.21.0.
If I use LSI with RTC I dont have problem.
But when I select LSE, program stuct at void _Error_Handler.
The problem is at this function.
while((hrtc->Instance->ISR & RTC_ISR_INITF) == (uint32_t)RESET)
{ if((HAL_GetTick() - tickstart ) > RTC_TIMEOUT_VALUE) { return HAL_TIMEOUT; } }I changed RTC_TIMEOUT_VALUE 1000 to 9000 but still I have problem.
I use stm32f429i discovery board (I had already soldered 32.762khz xtall) and
my .ioc file at link,
https://www.dropbox.com/s/jethyab2u0nuhih/akv_prjct.ioc?dl=0
Best regards
Celal HANCER