2019-10-22 02:08 AM
It's not possible to change the application structure in STM32CubeIDE v1.1.0.
STM32CubeMX v5.4.0 is installed.
The option "Advanced" is always used on every new created projects.
2019-10-22 02:55 AM
Hello @AScha.381 ,
Could you please share your ioc file ?
Thanks,
Khouloud.
2019-10-22 03:08 AM
2019-10-22 05:34 AM
You're right @AScha.381 , Issue will be fixed in the next release.
Thanks for bringing this bug to our attention .
Best Regards,
Khouloud
2019-10-22 05:46 AM
I'm glad to hear this.
Thank you very much for your support.
2019-10-22 08:51 AM
for the moment you can start your project from CubeMX 5.4.0 and set the basic advanced settings , then generate code with Toolchain CubeIDE.
Best Regards,
Khouloud.
2019-10-23 05:19 AM
Dear @AScha.381 ,
After discussed with team :
When starting the project, CubeIDE starts a “CubeMX�? project. And the project structure must be frozen at the beginning.
We have considered that it will be easier for our customers to start with a default “advanced�? structure, which is more “future proof�? for your design rather than to ask the enigmatic question to most of our customers. ( so maybe this will not be fixed in the next release :/ ).
Otherwise, if you need the basic Application structure* please start your project with CubeMX then generate CubeIDE code.
Best Regards,
Khouloud
2019-10-23 05:43 AM
Thank you for your help. Luckely I had an older IDE software installed and migrated a clean project to the newest project.
We regularly use the basic structure. I would be very grateful if the option will be available again in the next release.
2021-12-23 01:08 PM
This bug is not fixed yet. This option is just removed from the Code Generator page...