cancel
Showing results for 
Search instead for 
Did you mean: 

Availability in STM32CubeMX of use FreeRTOS with Memory Protection Unit (MPU) ?

Sebastien1
Associate II

Hello,

Currently, with 4.26.1 version, it is not possible to use special functions in FreeRTOS about the Memory Protection Unit (MPU).

I use the STM32F207VCT chipset with MPU functionality. Unfortunately, STM32CubeMX don't give me a way to use this functionality like, for example, MPU_xTaskCreateRestricted function.

There is the function header, but no code present.

It is too bad that have a important feature but I can't use it ...

Thanks in advance for the information.

Best regards.

2 REPLIES 2
Nawres GHARBI
ST Employee

Hi Sebastien,

Thanks for the feedback, your request has been been submitted to be added for a future release

rgree.8
Associate

Is there an ETA when this will be release?