cancel
Showing results for 
Search instead for 
Did you mean: 

Variable list under STM32 cube monitor remains inactive and hence no data update on chart

Nsg1987
Senior

I want to display ADC data on mychart -cube monitor. I found that varliable list remains inactive though it was made active under variables.

I dont know what is wrong.

1 REPLY 1
Richard.Chvr
ST Employee

Hello @Nsg1987 

On the attached image, I can see you've selected ADC1Samples[0] and pwm_start variable to be monitored.
Not sure to understand your issue, but if you want to edit this list, you need to click on the "pen" button.
Once you've selected/unselected the variable you want to monitor, click on "Update" button, then "Done".
Check that the list is also be updated in the processing node.

Don't forget to press deploy in order to validate your modification.

Feel free to come back to this community if needed and share your flow if possible.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.