2023-05-17 1:57 AM
I want to display ADC data on mychart -cube monitor. I found that varliable list remains inactive though it was made active under variables.
I dont know what is wrong.
2023-06-29 1:43 AM
Hello @Nsg1987
On the attached image, I can see you've selected ADC1Samples[0] and pwm_start variable to be monitored.
Not sure to understand your issue, but if you want to edit this list, you need to click on the "pen" button.
Once you've selected/unselected the variable you want to monitor, click on "Update" button, then "Done".
Check that the list is also be updated in the processing node.
Don't forget to press deploy in order to validate your modification.
Feel free to come back to this community if needed and share your flow if possible.