cancel
Showing results for 
Search instead for 
Did you mean: 

Where is the makefile generated by CubeIDE?

ubaldot
Senior

When I build a project I noticed that the command `make -j9 all` is run, which suggests me that there is Makefile somewhere, but it is not in my project folder. 

Does anybody know  where I can find it? 

I am working with a Nucleo-F446RE. 

1 ACCEPTED SOLUTION

Accepted Solutions
ubaldot
Senior

Ok. I found them in ./Debug and ./Release, depending on how you build your project. 

View solution in original post

10 REPLIES 10
ubaldot
Senior

Found! 

For the benefit of others who may come along with the same question, please describe where you found it.

And mark that as the Solution.

ubaldot
Senior

Ok. I found them in ./Debug and ./Release, depending on how you build your project. 

ubaldot
Senior

... however, when going into any of these two folders and running make all you get errors like 

arm-none-eabi-gcc: command not found

 

Probably because the IDE runs the makefile from its own internal "shell" - so you'd have to replicate that to make it work.

ubaldot
Senior

Any idea on how to do that? 

None at all!

Are you on Windows or Linux?

I think the IDE uses a Linux-like "shell"...

AScha.3
Chief III

I found this :

AScha3_0-1706028750975.png

and setting in project :

AScha3_1-1706028852888.png

seems not lying here:

AScha3_2-1706028894701.png

 

If you feel a post has answered your question, please click "Accept as Solution".
ubaldot
Senior

I am on macos. Yes, I also think so. Is there any way to open an interactive "cube shell" on CubeIDE?