cancel
Showing results for 
Search instead for 
Did you mean: 

When will cube IDE support the STM32H7 Dual Core processors / development boards? Are we going to be able to do proper dual core debugging with the ST Link 3 and STM32Cube IDE?

RAnde.14
Associate
 
3 REPLIES 3
Markus GIRDLAND
ST Employee

The team is working on the support for this right now.

Barring any catastrophic bugs that needs fixing this will be included in the next version of CubeIDE. I can't give more information than that at the moment.

PPete
Associate III

is there a release date for the new cubeide?

No, we have a specific one in mind that we are working towards but it's still early enough that the date could change so I'm going to need to keep it secret for now.