Using DSP libraries (e.g. arm_math.h) in STM32CubeIDE, STM32F4
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-27 11:43 PM
Hi I need some help,
I am having the same problem using CubeIDE v1.0. I have copied the arm_math.h, const_structs.h and arm_common_tables.h into Drivers/CMSIS/DSP/Include.
I was not able to find arm_math.h until I went to Project > Properties > C/C++ General > Paths and Symbols > Includes and added in Drivers/CMSIS/DSP/Include. That fixed the problem of not finding arm_math.h
After which I get a whole bunch of errors:
__uint32_t
../Drivers/CMSIS/DSP/Include/arm_math.h:6612:3: error: unknown type name 'uint32_t'; did you mean '__uint32_t'?
uint32_t blockSize);
...
...
../Drivers/CMSIS/DSP/Include/arm_math.h:6873:16: error: unknown type name '__STATIC_INLINE'
CMSIS_INLINE __STATIC_INLINE q15_t arm_bilinear_interp_q15(
^~~~~~~~~~~~~~~
../Drivers/CMSIS/DSP/Include/arm_math.h:6873:38: error: expected '=', ',', ';', 'asm' or '__attribute__' before 'arm_bilinear_interp_q15'
CMSIS_INLINE __STATIC_INLINE q15_t arm_bilinear_interp_q15(
^~~~~~~~~~~~~~~~~~~~~~~
../Drivers/CMSIS/DSP/Include/arm_math.h:6951:16: error: unknown type name '__STATIC_INLINE'
CMSIS_INLINE __STATIC_INLINE q7_t arm_bilinear_interp_q7(
^~~~~~~~~~~~~~~
Thanks!
- Labels:
-
DSP
-
STM32CubeIDE
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-28 12:09 AM
It seems that I need to define #ARM_MATH_CM4 in Project > Properties > C/C++ General > Paths and Symbols > Symbols. That will get rid of the errors above, but I will get a new error.
../Drivers/CMSIS/Include/core_cm4.h:105:8: error: #error "Compiler generates FPU instructions for a device without an FPU (check __FPU_PRESENT)"
#error "Compiler generates FPU instructions for a device without an FPU (check __FPU_PRESENT)"
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-28 12:10 AM
This seems to go away if I include main.h which includes "stm32f4xx_hal.h" before I include "arm_math.h"
Can someone confirm that this is the right way to include the DSP libaries?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-28 12:11 AM
For some reason in main.h, stm32f4xx_hal.h is included twice. Feels like a auto-generated bug?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-10 2:50 PM
#include "arm_math.h" STM32CubeIDE
I'm use CMSIS 5.4.0 My Directory C:\CMSIS_5-5.4.0\CMSIS\DSP\Include
poroject ->properties->C/C++ General->path and Symbols->Includes-> Add library directory
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-10 7:25 PM
yep I did that if you refer to my original post at the top. but I still faced some errors which I addressed in my following replies. Do you encounter them as well?
hmm, I guess my formatting for my original question may not be that clear. I have updated it to make it clearer.
Thanks for replying!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-07-21 1:12 PM
Did you get it working? I have the same problem.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-07-21 6:47 PM
yea, look at my comments above. still have stm32f4xx_hal.h included twice though.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-07-21 7:01 PM
I did what you explained and I keep getting this error:
I am using Nucleo-F767ZI
I have added ARM_MATH_CM7 with no value under the symbols
arm-none-eabi-gcc "../Drivers/CMSIS/DSP/Source/TransformFunctions/arm_bitreversal.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DSTM32F767xx -DDEBUG -DARM_MATH_CM7 -c -I../Inc -I../Drivers/CMSIS/Include -I../Drivers/CMSIS/Device/ST/STM32F7xx/Include -I../Drivers/STM32F7xx_HAL_Driver/Inc -I../Drivers/STM32F7xx_HAL_Driver/Inc/Legacy -I"C:/Users/alire/OneDrive/Desktop/New folder/1/Drivers/CMSIS/DSP/Include" -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Drivers/CMSIS/DSP/Source/TransformFunctions/arm_bitreversal.d" -MT"Drivers/CMSIS/DSP/Source/TransformFunctions/arm_bitreversal.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Drivers/CMSIS/DSP/Source/TransformFunctions/arm_bitreversal.o"
In file included from C:/Users/alire/OneDrive/Desktop/New folder/1/Drivers/CMSIS/DSP/Include/arm_math.h:319:0,
from ../Drivers/CMSIS/DSP/Source/TransformFunctions/arm_bitreversal.c:29:
../Drivers/CMSIS/Include/core_cm7.h:105:8: error: #error "Compiler generates FPU instructions for a device without an FPU (check __FPU_PRESENT)"
#error "Compiler generates FPU instructions for a device without an FPU (check __FPU_PRESENT)"
^~~~~
make: *** [Drivers/CMSIS/DSP/Source/TransformFunctions/subdir.mk:112: Drivers/CMSIS/DSP/Source/TransformFunctions/arm_bitreversal.o] Error 1
make: *** Waiting for unfinished jobs....
"make -j4 all" terminated with exit code 2. Build might be incomplete.
09:56:57 Build Failed. 3 errors, 0 warnings. (took 24s.614ms)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-07-21 7:08 PM
Actually my code throws different error if I change ARM_MATH_CM7 to ARM_MATH_CM4
when using M4 it says some functions are duplicates (ex. QSUB, SMLADX, SMLDX) and so on.