Unable to configure Clock using baremetal PLL in stm32 G071RB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-27 6:13 AM
i tried to configure clock by writing code in its appropriate registers...
following is the clock configuration function
furthermore,
when the Xtal frequency is greyed out as <undefined> in the dialog Options for target - Target tab. so I am unable to set the clock frequency to 64mhz
in the main.c code when I try to include this clock configuration, it fails to make any changes to the code and the simple led blink program fails to execute after flashing
following is my main.c file
Solved! Go to Solution.
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-27 11:08 PM - edited ‎2024-03-27 11:12 PM
Per the User Manual for the Nucleo-G071RB:
Further more you can configure the target to use MCO from STLink:
I modified your register level code to start up the HSI at 64MHz, this code woks and is tested, the rest of you code I did not implement:
void pwr_settings(void){
//enabling power interface
RCC->APBENR1 |= RCC_APBENR1_PWREN;
//configuring voltage regulator to default 01
PWR->CR1 |= (0x1UL << PWR_CR1_VOS_Pos);
PWR->CR1 &= ~(0x2UL << PWR_CR1_VOS_Pos);//
//configure flash prefetch and latency
FLASH->ACR |= (FLASH_ACR_ICEN | FLASH_ACR_PRFTEN | FLASH_ACR_LATENCY_1);
}
void SystemClockConfig(void){
#define PLLN 16
//using internal clock source
RCC->CR |= RCC_CR_HSION;
while(!(RCC->CR & RCC_CR_HSIRDY));
pwr_settings();
//configure main PLL; PLLM, PLLN, PLLR
RCC->PLLCFGR &= ~RCC_PLLCFGR_PLLN; // reset PLLN since it is NOT 0 on reset
RCC->PLLCFGR |= ((8<<RCC_PLLCFGR_PLLN_Pos) | (2<<RCC_PLLCFGR_PLLSRC_Pos));// use HSI , N=8
RCC->PLLCFGR &= ~RCC_PLLCFGR_PLLM; // M=1
RCC->PLLCFGR |= RCC_PLLCFGR_PLLR_0; // R=2
RCC->CR |= RCC_CR_PLLON; //enable PLL
RCC->PLLCFGR |= RCC_PLLCFGR_PLLREN; // enable PLLR output after PLL is enabled
while(!(RCC->CR & RCC_CR_PLLRDY)); //wait for PLL to be ready
//configuring prescalers for main clock and peripheral clocks
RCC->CFGR &= ~(RCC_CFGR_HPRE); // AHB prescaler to 1
// set system clock to PLL
RCC->CFGR |= RCC_CFGR_SW_1; // set system clock to PLL
// wait for pll to be used as sys clock, check for RCC_CFGR_SWS_1
while(!(RCC->CFGR & RCC_CFGR_SWS_1));
// set APB prescaler to 1
RCC->CFGR &= ~(RCC_CFGR_PPRE); // APB prescaler to 1
// update cmsis system core clock
SystemCoreClockUpdate(); // CMSIS defdined function to update SystemCoreClock variable
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-27 9:04 AM
I assume you see blinking with SystemClockConfig() commented out, and that you are aware of that 8x faster blinking may be too fast to see by eye.
I don't see anything fatal in your code.
Can you single-step the SystemClockConfig() code and observe the registers' content? Or at least, try variants with lighting up the LED at various points of SystemClockConfig() and see how far does it get.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-27 8:29 PM
Thanks for response,
I commented the SystemClockConfig() in main to verify if my blink code works by using just the timer6 configurations....and it did work that way...
when I tried to uncomment SystemClockConfig() and debug it, after stepping in line: RCC->CR |= RCC_CR_HSEON; it sets the HSEON bit in RCC_CR register to 1 but having the HSION and HSIRDY bit still 1 aswell
when i step into next instruction:while(!(RCC->CR & RCC_CR_HSERDY)); the code execution never leaves the loop and the debug is stuck in there as the RCC_CR_HSERDY bit does not set.....I believe this suggests that the clock is not switched to HSE
could advise on why this might be the issue?
my guess is that the clock frequency is not set accordingly and as I am unable to set it from Options for target - Target tab as Xtal frequency is greyed out as <undefined> I dont know how I can set the frequency to 64MHz before debug
any help would be appreciated
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-27 11:08 PM - edited ‎2024-03-27 11:12 PM
Per the User Manual for the Nucleo-G071RB:
Further more you can configure the target to use MCO from STLink:
I modified your register level code to start up the HSI at 64MHz, this code woks and is tested, the rest of you code I did not implement:
void pwr_settings(void){
//enabling power interface
RCC->APBENR1 |= RCC_APBENR1_PWREN;
//configuring voltage regulator to default 01
PWR->CR1 |= (0x1UL << PWR_CR1_VOS_Pos);
PWR->CR1 &= ~(0x2UL << PWR_CR1_VOS_Pos);//
//configure flash prefetch and latency
FLASH->ACR |= (FLASH_ACR_ICEN | FLASH_ACR_PRFTEN | FLASH_ACR_LATENCY_1);
}
void SystemClockConfig(void){
#define PLLN 16
//using internal clock source
RCC->CR |= RCC_CR_HSION;
while(!(RCC->CR & RCC_CR_HSIRDY));
pwr_settings();
//configure main PLL; PLLM, PLLN, PLLR
RCC->PLLCFGR &= ~RCC_PLLCFGR_PLLN; // reset PLLN since it is NOT 0 on reset
RCC->PLLCFGR |= ((8<<RCC_PLLCFGR_PLLN_Pos) | (2<<RCC_PLLCFGR_PLLSRC_Pos));// use HSI , N=8
RCC->PLLCFGR &= ~RCC_PLLCFGR_PLLM; // M=1
RCC->PLLCFGR |= RCC_PLLCFGR_PLLR_0; // R=2
RCC->CR |= RCC_CR_PLLON; //enable PLL
RCC->PLLCFGR |= RCC_PLLCFGR_PLLREN; // enable PLLR output after PLL is enabled
while(!(RCC->CR & RCC_CR_PLLRDY)); //wait for PLL to be ready
//configuring prescalers for main clock and peripheral clocks
RCC->CFGR &= ~(RCC_CFGR_HPRE); // AHB prescaler to 1
// set system clock to PLL
RCC->CFGR |= RCC_CFGR_SW_1; // set system clock to PLL
// wait for pll to be used as sys clock, check for RCC_CFGR_SWS_1
while(!(RCC->CFGR & RCC_CFGR_SWS_1));
// set APB prescaler to 1
RCC->CFGR &= ~(RCC_CFGR_PPRE); // APB prescaler to 1
// update cmsis system core clock
SystemCoreClockUpdate(); // CMSIS defdined function to update SystemCoreClock variable
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-28 12:45 AM
Thanks for your response...
I configured my clock for HSI and it works with precise delay....
appreciate for your help!