2024-08-21 09:09 AM - last edited on 2024-08-21 09:17 AM by Andrew Neil
Hi,
When using the linked-list DMA, there are two places show the 'Transfer Event Generation', one is in the 'GPDMA1' settings and the others in the 'LINKEDLIST' nodes settings. Are they refer to the same thing? If not, are there any reason to let user set them at two places?
Thanks.